SLYY231A March 2024 – March 2024 BQ25171-Q1 , BQ25622 , BQ25638 , LMQ66430-Q1 , LMR36502 , TPS37-Q1 , TPS62903-Q1 , TPSM365R15
Many battery-powered products such as power tools and e-bikes are characterized by the need to balance functionality and IQ in different power states. For example, a power tool in an active state (with the trigger pull on) may consume amperes of current, rendering the IQ of the battery monitor used in the power tool negligible with respect to the rest of the system. However, this same battery-powered power tool may be sitting on a table for hours or days in sleep mode, with basic protection features enabled. The power tool should also have the ability to respond quickly to a trigger pull. In such a low-power state, the IQ consumed by the BMS monitor becomes far more important.
By having a sleep mode that still has active protections; an enabled voltage regulator (to retain memory in the system microcontroller [MCU]); and duty-cycled voltage, current and temperature measurements through analog-to-digital converters, the system is still fully protected and ready to respond rapidly, while being able to cut power consumption by a factor of 10 or more relative to active mode. TI industrial monitors have a variety of sleep mode options, allowing you to choose whether to keep protections active (which lets you keep the discharge path enabled); the low-dropout regulator enabled (to allow the system MCU to retain memory and recover within microseconds instead of milliseconds); and duty-cycle options for voltage, current and temperature measurements for a safe, operational sleep mode that can be tailored to optimize power and performance.