SLYY231A March   2024  – March 2024 BQ25171-Q1 , BQ25622 , BQ25638 , LMQ66430-Q1 , LMR36502 , TPS37-Q1 , TPS62903-Q1 , TPSM365R15

 

  1.   1
  2.   Overview
  3.   At a glance
  4.   The importance of nano-IQ in different power applications
  5.   Achieving nano IQ in industrial BMS monitors
  6.   Achieving nano IQ in automotive BMS monitors
    1.     Achieving nano IQ in industrial home automation chargers
  7.   Achieving nano IQ in automotive BMS chargers
  8.   Achieving nano IQ in voltage supervisors
  9.   Achieving nano IQ in industrial and personal electronics DC/DC converters
  10.   Achieving nano IQ in automotive DC/DC converters
  11.   Conclusion
  12.   References
  13.   Additional resources

Achieving nano IQ in industrial home automation chargers

Our homes are getting smarter by using internet-connected devices to enable the remote monitoring and management of appliances and systems. The video doorbell, an essential smart home accessory, provides high-definition images and two-way audio communication so that homeowners can greet visitors from their smartphone. While most video doorbells are hardwired to a 12V to 16V supply, many consumers are seeking solar- or battery-powered video doorbells when the existing wiring or transformer is out of date or incompatible. The battery is normally very small to support wireless connectivity and the doorbell button press. TI’s BQ25622 and BQ25638 buck chargers have an IQ of 1.5µA in battery-only mode and 100nA in shutdown mode, with power path to maximize and extend battery run time throughout the product’s life cycle.

Enabling the essential functions of the device only when needed reduces IQ in these chargers, which have a function to monitor the battery temperature through the TS pin for safety reasons. As shown in Figure 2, a switch internal to the chip isolates the external thermistor network connected to the TS_BIAS pin from the 5V REGN pin. This architecture helps eliminate 99% of the thermistor bias current affecting charger IQ by enabling the internal switch with a 1% duty cycle.

GUID-20240226-SS0I-ZHL3-XCHJ-XZZ0KFGP0PM4-low.png Figure 2 TS_BIAS pin in the BQ25622 and BQ25638.

Turning off the system voltages while maintaining battery power in ship mode can reduce IQ even further. As shown in Figure 3, the BQ25622 and BQ25638 have an integrated, bidirectionally blocking internal field-effect transistor (FET) (Q4) that isolates the battery from the system in its off state. Ship mode is useful not only when the product is about to be boxed at the factory, but also when the device is low on battery, or when the user wants to power off the product.

GUID-20240226-SS0I-KJRH-XBNQ-ZXLKVQ9R3LBJ-low.png Figure 3 BQ25620 block diagram.