SNAA342 September 2020 LMX2820
The Voltage Controlled Oscillator (VCO) converts a tuning voltage to an output frequency. It has become increasingly popular to integrate these on integrated circuits along with other functionality. To achieve good phase noise performance and wide tuning range, the VCO frequency range is typically divided into several overlapping bands. This allows the individual bands to have lower VCO gain, which corresponds to better VCO phase noise. By adding all the bands together, they can jointly create a wide tuning range. For this technique to work, a calibration routine has to be used to tell the VCO which is the proper band to use for a given frequency.