SNAA390 july 2023 LMK6C , LMK6D , LMK6H , LMK6P
The plots shown in this section are captured before, during, and after the random vibration test, which are tested following the MIL-STD-883F method 2026C.
The capture data for the Z-axis movement of the DLE 4-pin (LVCMOS) oscillator is shown in Figure 3-15 and Figure 3-16.
The capture data for the Z-axis movement of the DLE 6-pin (LVPECL) oscillator is shown in Figure 3-17 and Figure 3-18.
The preceding plots show that the performance of the BAW Oscillator is robust during and after the vibration and the jitter performance is not degraded.