SNAK013 November   2022 LMK04832-SEP

 

  1.   Abstract
  2.   Trademarks
  3. 1Product Description
  4. 2Test Setup
    1. 2.1 SEL Test
    2. 2.2 SEFI Test
    3. 2.3 Test Facility
  5. 3Results
    1. 3.1 SEL Results
    2. 3.2 SEFI Results
  6. 4Summary
  7. 5References

SEL Results

SEL was not detected during the ion run. The supply current had some fluctuations due to ion strikes but the variation in current during the ion run was less than 1%. Any momentary increase in current was less than 1 mA. Occasionally the supply current dropped by up to 4 mA but would recover within microseconds. Supply current is plotted in Figure 3-1 .

Figure 3-1 Supply Current for the ion run LET at 48 MeV-cm2/mg and
DUT Board Thermister Reading of 125°C