SNAS648C October 2014 – February 2023 TDC1000
PRODUCTION DATA
CSB is an active-low signal and needs to be low throughout a transaction. That is, CSB should not pulse between the command byte and the data byte of a single transaction.
Deasserting CSB always terminates an ongoing transaction, even if the transaction is not yet complete. Reasserting CSB will always bring the device into a state ready for the next transaction, regardless of the termination status of a previous transaction.