SNAS650A JANUARY 2015 – September 2018 TPL5110
PRODUCTION DATA.
The TPL5110 can generate 1650 discrete timer intervals in the range of 100 ms to 7200 s. The first 9 intervals are multiples of 100 ms. The remaining 1641 intervals cover the range between 1 s to 7200 s. Because they are discrete intervals, there is a quantization error associated with each value.
The quantization error can be evaluated according to Equation 3:
REXT is the resistance calculated with Equation 1 and a, b, c are the coefficients of the equation listed in Table 1.