SNAS699B January 2017 – July 2019 LMK04610
PRODUCTION DATA.
The LMK04610 features a total of 10 PLL2 clock outputs driven from one of the internal VCOs.
All PLL2 clock outputs have programmable output types. They can be programmed to HSDS or HCSL.
If OSCout is included in the total number of clock outputs the LMK04610 is able to distribute up to 11 differential clocks.
The following sections discuss specific features of the clock distribution channels that allow the user to control various aspects of the output clocks.