SNAS717A April 2017 – October 2021 ADC12D1620QML-SP
PRODUCTION DATA
The input clock amplitude is specified as VIN_CLK in Converter Electrical Characteristics: AC Electrical Characteristics. Input clock amplitudes above the maximum VIN_CLK may result in increased input offset voltage. This causes the converter to produce an output code other than the expected 2047/2048 when both input pins are at the same potential. Insufficient input clock levels result in poor dynamic performance. Both of these results may be avoided by keeping the clock input amplitude within the specified limits of VIN_CLK.