SNAS724A February 2018 – April 2018 LMK05028
PRODUCTION DATA.
After device POR configuration and initialization, the APLL will automatically lock to the XO clock once it is detected by its input monitor. The output clock frequency accuracy and stability in free-run mode are equal to that of the XO input. If the TCXO input is used, the TCXO-DPLL will lock to the TCXO/OCXO clock once it is detected by its input monitor, and the output clock frequency accuracy and stability in free-run mode are equal to that of the TCXO/OCXO input. The reference inputs remain invalid (unqualified) during free-run mode.