SNAS724A February 2018 – April 2018 LMK05028
PRODUCTION DATA.
The EEPROM array is non-volatile memory mapped directly from the SRAM array.
After the register settings have been written to SRAM (by either Method #1 or #2), the EEPROM can be programmed through the following sequence:
On the next power-up or hard reset, the device can self-start in EEPROM mode from the newly programmed configuration. Also, the NVMCNT register value will be incremented by 1 after power-up or hard reset to reflect total number of EEPROM programming cycles completed.