SNAS785D November 2019 – March 2022 LMX2694-EP
PRODUCTION DATA
The SYNC pin allows the user to synchronize the LMX2694-EP such that the delay from the rising edge of the OSCIN signal to the output signal is deterministic. Initially, the devices are locked to the input, but are not synchronized. The user sends a synchronization pulse that is reclocked to the next rising edge of the OSCIN pulse. After a given time, t1, the phase relationship from OSCIN to fOUT will be deterministic. This time is dominated by the sum of the VCO calibration time, the analog setting time of the PLL loop, and the MASH_RST_CNT if used in fractional mode.
When the SYNC feature is enabled, part of the channel divide may be included in the feedback path.
OUTx_MUX | CHANNEL DIVIDER | IncludedDivide |
---|---|---|
OUTA_MUX = OUTB_MUX = 1 ("VCO") | Don't care | 1 |
All other valid conditions | Divisible by 3 but NOT 24 or 192 | SEG0 x SEG1 = 6 |
All other values | SEG0 x SEG1 = 4 |