SNAS854 February 2023 TDC1000-Q1
PRODUCTION DATA
The STOP pulse generation block of the TDC1000-Q1 contains two auto-zeroed comparators (a zero-cross detect and a threshold-detect comparator), a threshold setting DAC, and an event manager.
Comparator auto-zero periods occur at the beginning of every TOF receive cycle. During these periods, the input offset of the comparator is stored in an internal 2.5-pF capacitor, and the offset is subtracted from the input signal during the echo processing phase. The duration of auto-zero period is configured with the AUTOZERO_PERIOD field located in the CLOCK_RATE register.