SNAS854 February 2023 TDC1000-Q1
PRODUCTION DATA
In Mode 1 the TDC1000-Q1 associates each transducer to a single TX and RX channels. The transmit/receive pair "TX1/RX1" will act as both transmitter and receiver for a measurement if CH_SEL = 0. The transmit/receive pair "TX2/RX2" will act as both transmitter and receiver for the measurement if CH_SEL = 1.
The TDC1000-Q1 performs a single TOF measurement (one direction) and returns to the SLEEP mode when the measurement is complete.