If you haven’t done so, connect the USB cable from the MSP430 Launch Pad to your PC.
If you haven't done so, connect the TDC7201EVM to the MSP430 Launch Pad via J1 and J2 as shown in Figure 6.
Setting the Dual Channel Function Generator:
Set channel 1 of the dual function generator to the following (see Figure 5):
Pulse 1-Cycle
Burst mode
Freq = 40 kHz
Delay = 0 s
Amplitude = 3.3 Vpp
Offset = 1.65 V
Duty = 20%
Burst Trigger Source = External
Set channel 2 of the dual function generator to the following (see Figure 5):
Pulse 1-Cycle
Burst mode
Freq = 40 kHz
Delay = 19 µs --> this is the time-of-flight (TOF)
Amplitude = 3.3 Vpp
Offset = 1.65 V
Duty = 20%
Burst Trigger Source = External
Figure 5. START and STOP Signals Scope Shot
Connecting the Input Signal:
Using a USB-to-SMA cable, connect channel 1 of the dual function generator to TDC7201EVM’s START1_EXT connector (J5).
Using a USB-to-SMA cable, connect channel 2 of the dual function generator to TDC7201EVM’s STOP1_EXT connector (J4). See Figure 6.
Connecting the Trigger Input:
Connect DTG_TRIG (TP9) to the TRIGG input of the dual function generator. DTG_TRIG is generated by the MCU whenever a new measurement is started by the TDC7201. See Figure 6 and Figure 7.