SNAU263A February 2022 – July 2022
To use the DCO shift controls on a given APLL, enter the DCO ppb step value into the DCO Step Size (ppb) box shown below. The entered step size will be used to calculate a numerator deviation and a 2s complement numerator deviation. To perform the shift, the increment or decrement button must be pressed. An increment will write the numerator deviation to the DPLLx_FREE_RUN control which will result in a positive frequency shift in the amount specified by the DCO Step Size (ppb). An decrement will write the 2s complement numerator deviation to the DPLLx_FREE_RUN control which will result in a negative frequency shift in the amount specified by the DCO Step Size (ppb).
The slew rate at which the adjustment will occur is set on the DPLLx_HOLD_SLEW_STEP control. Ensure the DPLLx_HOLD_SLEW_STEP is NOT equal to 0, otherwise the adjustment will not occur. Recommended DPLLx_HOLD_SLEW_STEP value is 63 (maximum value). A value of 63 will result in the fastest adjustment.