SNAU265C june 2021 – july 2023 HDC3020 , HDC3020-Q1 , HDC3021 , HDC3021-Q1 , HDC3022 , HDC3022-Q1
Auto Measurement mode is a continuous operation mode. The user can select the measurement frequency between 10 samples a second to 1 sample every 2 seconds.
To configure the device to collect both the humidity and temperature data in continuous mode, select the desired Auto Measurement mode and low power mode duration from the command table. To obtain the temperature and humidity values, the user can issue commands 0x0E & 0x00. After placing the device into the auto measurement mode desired (Table 8-3 in theHDC3020 data sheet), the user should issue command code 0xE0 0x00 at coinciding time intervals to read out the temperature and relative humidity measurement values.