SNAU270 February 2022 LMK1D1208I
The LMK1D1208I can receive either a differential or single-ended clock as input. The default board configuration is for an LVDS differential signal at both device inputs. The inputs can be applied through the SMAs: J1, J2 (IN0_P, IN0_N) or J3, J4 (IN1_P, IN1_N). These inputs are AC-coupled to the device. The common-mode voltage is provided by the device on-chip bias generator (VAC_REF pins), which can be measured at TP1 and TP2.