SNAU273 December   2022 LMX2820

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2SYNC Category
  5. 3SYNC Examples
    1. 3.1 Category 1 SYNC Example
    2. 3.2 Category 2 SYNC Example
    3. 3.3 Category 3 SYNC Example
  6. 4Other Considerations When Using SYNC
  7. 5References

SYNC Category

The requirements for phase synchronization depend on certain LMX2820 setup conditions. To use phase synchronization, first determine the SYNC category using the flow chart below.

Figure 2-1 SYNC Category Flow Chart

For Category 1 SYNC, there is no restriction at all. We do not need to enable SYNC mode (that is, we can keep register PHASE_SYNC_EN = 0). A SYNC signal is also not required.

In Category 2 SYNC, we must make PHASE_SYNC_EN = 1 and provide a SYNC signal to LMX2820. The SYNC signal is not time-critical, therefore a Low-to-High transition at the PSYNC pin is good enough.

When the LMX2820 configuration falls into Category 3 SYNC, we need both PHASE_SYNC_EN = 1 as well as a time-critical SYNC pulse. The setup and hold time of the SYNC pulse as specified in the data sheet must obey.

Figure 2-2 Time Critical SYNC Pulse

From the data sheet, the minimum tCS and tCH is 2.5 ns and 2 ns, respectively. Furthermore, the maximum fOSCIN is restricted to 200 MHz.

A reliable phase synchronization is not possible if the configuration of LMX2820 does not fall into the above categories.