Table 2-1 describes the default jumper positions for the EVM to power the device from a single 12-V supply provided to VIN4. In positional information about jumpers, "opposite designator” means the jumper is placed opposite of the silkscreen designator.
Table 2-1 Default Jumper and DIP Switch Settings
CATEGORY
REFERENCE
DESIGNATOR
POSITION
DESCRIPTION
Power
JP1
1-2 (opposite designator)
LMK5B33414 VDD = 3.3 V from DCDC1 provided by U500 on top of the PCB.
JP2
1-2 (opposite designator)
LMK5B33414 VDDO = 3.3 V from DCDC1 provided by U500 on top of the PCB.
JP4
1-2 (opposite designator)
XO VCC = 3.3 V DCDC1 provided by U500 on top of PCB.
Communication
JP5
1-2, 3-4
Connect I2C from onboard USB2ANY to LMK5B33414
LMK5B33414 Control Pins
S3
S3[1:2] = OFF
SCS_ADD = no pullup or pulldown.
S1, S2, S4
Sx[1,2] = OFF
Sx[3,4] = ON
Enable 3.9 kΩ pulldown on GPIO0, GPIO1, and GPIO2
To begin using the LMK5B33414, follow the steps below.
Hardware Setup
Verify the EVM default jumper and DIP switch settings shown in Figure 1-1.
Connect the 12-V external power DC power supply (1-A limit) to:
VIN4 and GND terminals on header J500 (pins 4 and 5, see Figure 3-2.)
Connect references:
25-MHz reference clock to IN0_P/N and/or,
25-MHz reference clock to IN1_P/N
Connect the USB cable to the USB port at J41.
Software Setup
If not already installed, install the TICS Pro software from the TI website: TICS Pro Software
If the MATLAB R2015b (9.0)* 64-bit Runtime is not already installed, download and install the software from the MathWorks website. While optional for programming and evaluating the default profile settings, Matlab Runtime is necessary for any application that needs to modify the DPLL loop filter settings. See Matlab Runtime.
Start the TICS Pro software.
Select the LMK5B33414 profile from Select Device → Network Synchronizer Clock (Digital PLLs) → LMK5B33414.
Confirm communications with the board by:
Click USB communications from the menu bar.
Click Interface to launch the Communication Setup pop-up window.
Check these fields in the Communication Setup pop-up window:
Ensure USB2ANY is selected as the interface.
In case of multiple USB2ANY, select desired interface. If a USB2ANY is currently in use in another TICS Pro, you must release that interface by changing its interface setting to DemoMode.
Click Identify to trigger the LED shown in the image below. A blinking LED confirms you are connected to the board you expect. Be aware that USB2ANY devices connected to the PC but not attached to by a TICS Pro instance may blink at a slow rate of 1 second on, 1 second off, continuously. After clicking the Identify button, the LED will flash quickly at about 0.5 seconds on, 0.5 seconds off, for about 5 seconds.
Figure 2-1 USB LED.
Program the LMK5B33414
Toggle the switch S5 (PDN/RESET).
Program all the registers:
Press the Write All Regs button in the toolbar.
Select USB Communications in the menu bar, then select Write All Registers, or press Ctrl + L.