The on-board USB2ANY interface provides a bridge between TICS Pro software and the
LMX1906-SP device. When the on-board USB2ANY controller is first connected to a PC,
or if the firmware revision for the controller does not match with the version used
by TICS Pro, a firmware update to the controller is required.
- Connect the USB cable from the PC
to the EVM. The USB interface provides the necessary power to enable the
on-board USB2ANY controller.
- After Windows has set up a
USB device, run TICS Pro in the PC.
- The next screen looks like the
image below.
- Click OK, then the screen
looks like the image below. Click Update Firmware.
- Then the screen below
appears.
- Click the Close button to
close the window.
- A TICS
Pro default device pops up. Check to make sure that we get a green light on
Connection Mode at the bottom of the GUI.
- Go to the menu bar, click USB
communications, then select Interface.
- Click the Identify button,
the LED in the USB2ANY interface flashes.
- Now, the USB2ANY is ready to use.
Click the Close button to close the window.