SNAU291A October 2023 – September 2024
Automatic output disable (AOD) can be enabled or disabled using this control. AOD is enabled by default on LMKDB1108. AOD disables the outputs when low when there is a loss of signal (LOS) detected on the input. When AOD is disabled, outputs follow the input clock in DC state.