SNAU296 December 2023 LMK5C33414A
Set the clock input select mode for the DPLLs, input priority, and maximum TDC frequency. The recommended Input Select Mode is Auto Revertive. REF0, REF1, REF2, and REF3 shown below correspond with IN0, IN1, IN2, and IN3, respectively. REF4 and REF5 priorities can be set if the DPLLs input is fed from one of the APLL post divider frequencies. The corresponding APLL is listed next to the REF4 and REF5. The REF with the highest priority is fed as the DPLL input.