By default, the LMKDB1120 and the GUI
are started with the default configuration. When using the on-board USB supply
option, the following steps can be followed to avoid any improper power up sequence
issues when plugging the USB calculate to the EVM.
- After all the steps above, toggle
the USB 3V3 Supply pin Low → High for power reset. This
step is not necessary but recommended if there are any issues with the readback
or improper start up on EVM.
- Click on Scan Bus in the
Communication Setup window to find and update device address.
- Click on Read All Regs to
update the register readback from the device.