The LMKDB1120 has 16 different slew
rates options that can be assigned to the outputs. 0x0 is the fastest slew rate
setting and 0xF is the slowest slew rate setting. To set the slew rate of each
output, follow these steps:
- There are four different registers, SLEWRATE_OPT#, that can
store up to four different slew rates. Select your desired slew rates by
assigning a value from 0x0 (fastest) to 0xF (slowest) to each SLEWRATE_OPT#
register. The default values set to each SLEWRATE_OPT# register can be found in
Table 4-3.
- For example, if you wanted the fastest, second
fastest, and the slowest slew rate, assign 0x0, 0x1, and 0xF to
registers SLEWRATE_OPT#. SLEWRATE_OPT1 = 0x0 (fastest), SLEWRATE_OPT2 =
0x1 (second fastest), and SLEWRATE_OPT3 = 0xF (slowest). SLEWRATE_OPT4
does not have to be assigned, but if you want more than one register set
to a slew rate, then SLEWRATE_OPT4 can be assigned to any of the three
previous settings. For this example, SLEWRATE_OPT4 = 0xF (slowest) as
shown in Figure 4-4.
Table 4-3 Default SLEWRATE_OPT_#
Values
Register Field Name |
Default Value |
Default Slew Rate |
SLEWRATE_OPT_1 |
0x0 |
Fastest |
SLEWRATE_OPT_2 |
0x6 |
Fast |
SLEWRATE_OPT_3 |
0xA |
Slow |
SLEWRATE_OPT_4 |
0xF |
Slowest |
- Set a slew rate for each output by using the drop-down menus
under the Output Slew Rate Control Section. The default SLEWRATE_OPT#
register assignment for all outputs is SLEWRATE_OPT2, which has a default slew
rate of 0x6.
- Following the example
from step 1a, if you wanted CLK0, CLK1, CLK2, and CLK3 to have the
fastest slew rate, CLK4 and CLK7 to have the slowest slew rate, and CLK
5 and CLK6 to have the second fastest slew rate, set the drop-down menus
of CLK0, CLK1, CLK2, and CLK3 to OPT_1, CLK4 and CLK7 to OPT_3 or OPT_4,
and CLK5 and CLK6 to OPT_2 as shown in Figure 4-5.
Repeat this step to set the slew rate of the other 12 outputs.