SNIA053 june 2023 TMP61-Q1
Figure 2-1 shows the TIDA-020030 hardware and the IGBT module with double-sided cooling. The position of the isolated gate driver, UCC21732-Q1, is also shown. The heat sinks are symmetrically attached to the top and bottom side of the IGBT module for maximum cooling. The isolated barrier on the drive board is outlined by the PCB silkscreen.
Additionally, the following laboratory test equipment is used: