SNIS232A October 2023 – June 2024 ISOTMP35
PRODUCTION DATA
The ISOTMP35 can support either a step input power supply or a ramp power supply. When powering the device, consider the analog output settling time upon start-up. For a step VDD input, start-up time is approximately 1ms.
The ISOTMP35 can support either a step input power supply or a ramp power supply. When powering the ISOTMP35, the user must keep in mind that the ISOTMP35 requires time to settle the analog output upon start-up:
See Figure 5-8 and Figure 5-9 for more information.