SNIU039 December   2019

 

  1.   HDC2022EVM User's Guide
    1.     Trademarks
    2. 1 Quick Start
    3. 2 EVM GUI
      1. 2.1 Software Setup
        1. 2.1.1 Live Software on dev.ti.com
        2. 2.1.2 Offline Software
          1. 2.1.2.1 Download GUI from dev.ti.com
    4. 3 GUI Operation
      1. 3.1 Home Tab
      2. 3.2 Data Capture Tab
      3. 3.3 EVM Settings Tab
      4. 3.4 Device Configuration
      5. 3.5 Registers Tab
      6. 3.6 Collateral Tab
    5. 4 EVM Hardware
      1. 4.1 Input/Output Connector Description
        1. 4.1.1 J1 & J2 – 5x1 Headers
        2. 4.1.2 USB Type A Connector
      2. 4.2 EVM Operating Conditions
      3. 4.3 Device Address Configuration
      4. 4.4 Reducing the Sensor's Thermal Mass
    6. 5 Updating Firmware on HDC2022EVM
    7. 6 Board Layout
    8. 7 Schematic
    9. 8 HDC2022EVM Bill of Materials

Data Capture Tab

The Data Capture tab reports the temperature and humidity from the HDC2022 device included on the HDC2022EVM. To enable data capture, ensure that an auto-read delay from the drop down menu at the top of the page is selected.

Each selection option/button on this tab has a specific function as described below:

  • Register Auto Read Delay: Changes the delay between register reads
  • Measurement Configuration: Configures the HDC2022 to return temperature, humidity, or both.
  • Humidity/Temperature Resolution: Change the number of measurement bits for humidity/temperature measurements.
  • Auto Measurement Mode: Set the auto-measurement frequency of the HDC2022.
  • Start Measurement/One-Shot Button: In shutdown mode, this button triggers a measurement. When an auto-measurement frequency is selected, this button begins measuring from the HDC2022.
  • Celsius/Fahrenheit Select: Sets the GUI to display in Celsius or parenthetic. This does not change settings for the HDC2022 or EVM.
  • Activate Soft Reset Button: Triggers a soft reset of the HDC2022.
  • Activate Heater Button: Enables the heater on the HDC2022.

SNIU039_DataCaptureTab.pngFigure 5. Data Capture Tab of HDC2022EVM GUI