SNLA132G October 2011 – November 2020 DS90UB928Q-Q1 , DS90UB941AS-Q1 , DS90UB948-Q1 , DS90UH925Q-Q1 , DS90UH926Q-Q1 , DS90UH940N-Q1
The DS90Ux928Q-Q1 and DS90UB924-Q1 deserializers require an extra configuration step to use their internal clock source. Note that this step is unnecessary if the pixel clock is derived externally (that is received from the serializer). Before enabling the Internal Test Pattern Generator with an internal pixel clock source, configure the register shown below:
ADD(hex) | Register Name | Bit | Access | Default (hex) | Function | Description |
---|---|---|---|---|---|---|
0x39 | PG Internal Clock Enable | 7:2 | 0x00 | Reserved | ||
1 | RW | PG INT CLK | Enable Pattern Generator Internal Clock This bit must be used to set the Pattern Generator Internal Clock Generation 0: Pattern Generator with external PCLK 1: Pattern Generator with internal PCLK |
|||
0 | Reserved |