This application note includes how to setup and configure the DP83867 and DP83869 (further refereed to as DP8386x) PHY for Ethernet Physical Layer Compliance (IEEE802.3). This application note primarily uses DP83867 as an example, but DP83869 can also use these scripts for compliance testing.
While the same 10/100 Mbps testing methodology is used in the exclusive 10/100 Mbps PHYs (DP83822, DP83825, DP83826), please refer to DP8382x IEEE 802.3u Compliance and Debug, application note for more detailed procedure specific to those devices.