The following section mainly go over the general
guideline on how to debug compliance issue on DP83867PHY.
- Check the schematic
- Make sure the Transformer
follow data sheet specification in Section 2.3.1.
- No shorted center taps on
transformer
- Double check on the
capacitors on the center taps of transformer
- Remove ESD diodes on MDI
lines for compliance test
- Check Rbias value and
make sure the value falls in the 1% range
- Follow the schematic
check list recommendation in Section 2.2
- Check the layout
- Make sure no clock signal
and data signal near the MDI lines
- Check length matching and
impedance matching (100ohms) for MDI lines
- No vias around the MDI
lines
- Follow the layout
checklist in Section 2.2
- Check the compliance test
How to Configure DP8386x for Ethernet Compliance
Testing application note. Follow the procedure on the
compliance test application note.