SNLA267A March 2019 – June 2019 DS90UB953-Q1 , DS90UB954-Q1 , DS90UB960-Q1
FPD-Link III devices such as the DS90UB95x-Q1 can support cameras in Advanced Driver Assist Systems (ADAS) in the automotive industry. There are complications that can occur in system implementation due to the complexity of the technology, so it is important to ensure proper design. The purpose of this document is to systematically design a SERDES system using the DS90UB953-Q1 and DS90UB954-Q1.
All other trademarks are the property of their respective owners.
The DS90UB954-Q1 FPD-Link III deserializer, in conjunction with an ADAS FPD-Link III serializer, supports the video transport needs with an ultra-high-speed forward channel and an embedded bidirectional control channel. After the DS90UB954-Q1 receives the data, the device outputs the data from a configurable MIPI CSI-2 port. The CSI-2 port may be configured as either a single CSI-2 output with four lanes up to 1.662 Gbps per lane, or as two 2-lane CSI-2 outputs that can send replicated data on both ports. The engineer can use a second differential clock for the second replicated output when the device is configured for dual CSI-2 outputs that can support one clock lane and one or two data lanes each. The DS90UB954-Q1 can support multiple data formats and different resolutions as provided by the sensor. Conversion between different data formats is not supported. The CSI-2 Tx module accommodates both image data and non-image data (including synchronization or embedded data packets).
The DS90UB953-Q1 serializes data from high-resolution image sensors or other sensors using the MIPI CSI-2 interface. The DS90UB953-Q1 serializer is optimized to interface with the DS90UB954-Q1 deserializer (dual hub) or the DS90UB960-Q1 deserializer (quad hub) as well as potential future deserializers. The interconnect between the serializer and the deserializer can be either a coaxial or shielded twisted-pair (STP) cable. The DS90UB953-Q1 was designed to support multi-sensor systems such as surround view, and as such has the ability to synchronize sensors through the DS90UB954-Q1 and DS90UB960-Q1 hub.
Due to the complexity of this system, there are a variety of issues that can be avoided by proper design. The purpose of this guide is the help the user systematically design a system using the 953 and 954. The following chapters show the typical concepts and tests and how to implement them. This guide lists basic design rules as a checklist that should be followed to ensure proper initialization of the system. The items described in the suggested checklist are the building blocks of the system. Without them, the system will not work as expected.
Following the completion of the basic design rules section, this guide provides analysis of the three important links in the ADAS System using DS90UB953-Q1 and DS90UB954-Q1:
Important procedures and design considerations are highlighted and explained in the form of script examples, general steps, and flow charts.
At the end of this guide is a set of hardware design topics that are commonly discussed when designing a SERDES system.