SNLA308A April 2019 – October 2020 DS90UB941AS-Q1 , DS90UH941AS-Q1
In addition to the cropping options, the Horizontal Sync width and Horizontal Back Porch period may be modified. Front Porch value may be determined from total line length - (Active line length + Horizontal Back Porch + Horizontal Sync). Typically, these values are automatically generated based on the input video (half of the values in the dual image), but these can be overridden by setting the IMG_HSYNC_CTL registers. The Horizontal Sync period and the Horizontal Back Porch can be individually overridden by setting the HSYNC_OV_EN or HBACK_OV_EN controls, as well as the IMG_HSYNC and IMG_HBACK parameters. When overriding the IMG_HBACK parameter, the resultant back porch is half of the programmed value, rounded up, plus one extra pixel. When overriding the IMG_HSYNC parameter, the resultant sync width is half the programmed value, rounded up. If the HSYNC and HBACK values are reduced, then the difference is added to the horizontal front porch. If the HSYNC and HBACK values are increased, then the difference is subtracted from the horizontal front porch.