SNLA308A April 2019 – October 2020 DS90UB941AS-Q1 , DS90UH941AS-Q1
VIDEO_3D_STS is described in Table 3-1.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7-3 | RESERVED | R | 0h | Reserved |
2 | LINE_OV_ERR | R/RC | 0h | Line Buffer Overflow: When set to a 1, an error has been detected in the 3D video line buffers due to receiving a video line that was too long for the buffer. For Alternate Line 3D mode, this flag is set if a video line contains 4096 or more pixels. For Left/Right 3D, or Alternate Pixel 3D modes, this flag is set if a video line contains 8192 or more pixels. This flag will be cleared on read. |
1 | LINE_VID_ERR | R/RC | 0h | Line Video Error: When set to a 1, an error has been detected in the 3D video processing likely due to invalid line length or blanking intervals. This flag is cleared on read. |
0 | LINE_MISMATCH | R/RC | 0h | Line Mismatch Error. Alternate Line 3D mode: When set to a 1, odd or even video line length mismatch has been detected. This occurs if the odd and even lines of a video are note the same length. This flag is cleared on read. Left/Right 3D mode: When set to a 1, a line length error has been detected. This occurs if the received video line is not twice the IMG_LINE_SIZE value. If the received line length is less than IMG_LINE_SIZE, an error may not be detected. This flag is cleared on read. If the image is cropped in the horizontal dimension, this error flag may not be accurate. |