SNLA356 September 2020 DS90UB941AS-Q1 , DS90UH941AS-Q1
The MIPI D-PHY v1.2 receiver specification requires the sink device to ignore activity on the DSI data lanes at the end of high speed packet transmission prior to re-entering the low power state (LP-11) in order to mask transition effects during the End of Transmission (EoT) sequence. If the THS-SKIP timing parameter is mis-configured, it may result in data errors in the DSI video stream.
Symptoms:
Resolution:
DS90UB941AS-Q1 requires user configuration of the tHS-SKIP timing parameter based on the DSI clock speed applied. The TSKIP_CNT (dec) value is defined in Equation 14, where fDSI is the DSI clock frequency in GHz.
This value must get loaded into DS90UB941AS-Q1 register 0x05[6:1] (in hex) prior to enabling the DSI receiver.
To program TSKIP_CNT, use the following programming steps via I2C:
The DS90Ux941AS-Q1 Superframe Design Calculator tool is available in the DS90UB941AS-Q1 product folder, which also includes calculations for TSKIP_CNT.