The DSI transmitter must convey
accurate DPI-type timing for HSS, and VSS packets as well as the pixel transmission
rate for each active line to match the desired video timing.
Since Event Mode does not utilize HSE
and VSE packets to define the falling edge of the HSYNC/VSYNC signals, the
serializer must be programmed to generate the desired sync widths with the
DSI_HSW_CFG and DSI_VSW_CFG registers.
The timing of the rising edge of each
sync signal is defined by the received timing of the HSS/VSS DSI short packets
(which also defines the horizontal and vertical back porch value for the
video).
The output pixel rate can be defined
by the DSI clock rate in continuous clock mode or by the REFCLK source applied to
the DS90UB941AS-Q1.
Figure 2-2 Non-Burst Mode with Sync Events
Packet Structure.