SNLA399 July 2022 OPA607
The filter response of this circuit is a bandpass filter composed of simple poles and zeroes. The passband frequency range of the signal chain is from 0.1 Hz to 1 kHz as shown in Figure 2-2. The upper cutoff frequency is important to restrict the noise bandwidth of the circuit. The lower cutoff frequency is required to remove DC offset.
The feedback capacitance (Cf = 1.5 pF) in parallel to the feedback resistor (Rf = 60 MΩ) is required to avoid any instability issues in the TIA. For details on stabilizing a TIA using feedback capacitance see What You Need To Know About Transimpedance Amplifiers – Part 1. The feedback network generates a pole given by,
The RC low pass filter placed at the output of operational amplifier increases the fall off rate to 40 dB/dec helping in reducing the output voltage noise thereby, improving the SNR. The RC low pass filter (roll-off filter) gives a pole at frequency given by,
The two poles around 1.6 kHz results in a 3 dB point around 1 kHz. Therefore, the upper cutoff frequency of the AFE settles to 1 kHz.
The high pass filter at the operational amplifier output end removes the DC offset due to diode dark current, input bias current and offset voltages of the operational amplifier. Thus only the photo current pulses due to the presence of particle are digitized using ADC. This helps in making the calibration algorithm independent of DC offsets.
A high pass RC filter, inserts a zero at origin and a pole at high pass cutoff frequency which can be adjusted using,
The particle flow rate range requirement of the PM sensor relates to passband frequency range of AFE. Maximum flow rate of particles sets limit for upper cutoff frequency and minimum flow rate sets the lower cutoff frequency,