SNLA426 june 2023 DS320PR1601 , DS320PR410
When routing differential signals across common PCB materials, each trace experiences different dielectric constants and corresponding signal velocities due to the differences in static permittivity (εr) of the fiberglass weave (εr is approximately 6) and epoxy (εr is approximately 3) that comprise a PCB. Differences between εr and loss tangent (Df) are caused by holes or openings within the fiber glass laminate. These differences cause resonance or anti-resonance in return loss or the insertion loss of the transmission media at different frequencies across the signal bandwidth.
A signal travels faster when εr is lower; therefore, an intra-pair skew can develop if a signal in a differential pair travels over a higher ratio of fiberglass or epoxy than the companion signal does. This intra-pair skew starts appearing on SDD12 and SDD22 at 2GHz and higher. This skew between the differential signals can significantly degrade the differential eye diagram as presented to the receiver, causing significant duty cycle distortion, AC common-mode voltage noise, and EMI issues. The extent of this problem will depend on the data rate, the length of the traces, the trace geometries, the type of fiberglass weave used, and the alignment of the traces to the weave pattern of a PCB. Problems from fiber weave alignment vary from board to board. This variance makes issues difficult to diagnose.
εr typically ranges from 2.5 to 4.5 and varies with frequency – decreases as frequency increases. Df is a measurement of material power dissipation or the degree of signal attenuation and typically ranges from 0.02 to 0.001 for ultra-low loss materials. Smaller values of Df result in lower signal attenuation, thus a low Df is desirable for high speed applications such as PCIe.
Figure 8-1 and Figure 8-2 show the two most common methods to minimize the impact of PCB fiber weave in a board design. The goal of each method is to ensure that both signals of the differential pair will share a relatively common across the length of the pair routing.
The entirety of the signaling image plane is rotated 10° to 35° in relation to the underlying PCB fiber weave. The PCB manufacturer can affect this rotation without making changes to the PCB layout database as shown in Figure 8-1.
The high-speed differential signals are routed in a zig-zag fashion across the PCB as shown in Figure 8-2
Because the ratio of fiberglass to epoxy is the primary contributor to the εr disparity, choose a PCB style with a tighter weave, less epoxy, and greater εr uniformity across longer trace lengths. Before sending the design out for fabrication, specify a PCB style that can best accommodate high-speed signals.