SNLA431 January 2024 DP83TC812R-Q1 , DP83TC812S-Q1
Incorrect strap configurations are one of the most common issues leading to lack of data throughput. For example, if the incorrect MAC interface mode is chosen or the PHY is placed in managed mode when autonomous mode is intended to be used, data transmission and reception is not successful.
The strap values sampled at power up can be read from register 0x45D (CHIP_SOR_1) using Extended Register Access. Use the strap tool in the DP83TC812 Schematic Checklist to verify the intended straps configuration has been loaded in register 0x45D.
Verify that the MAC is not driving any pins connected to the PHY upon power up or reset pin de-assertion. This causes an incorrect voltage to be sampled and cause the strap value to be different than intended. All MAC pins connected to the PHY must be placed in a High-Z state while the PHY is powering up or coming out of reset.