SNLA443 December 2023 DP83869HM
DP83869HM is capable of 100Base-FX and 1000Base-X fiber communication. When using fiber, speed is not determined by auto-negotiation. Both sides of the link must be configured to the same operating speed. The pins used for fiber are also the same pins used for SGMII: SIP/SIN and SOP/SON. The DP83869HM must be set to either SGMII to Copper or RGMII/MII to fiber. A SGMII to fiber connection is not possible.
Pin | I/O | Type | Description | |
---|---|---|---|---|
NO. | Name | |||
14 | SON | O | Analog | Differential SGMII or Fiber Data Output: This signal carries data from the PHY to the MAC, fiber transceiver, or link partner in SGMII and fiber modes. This pin is AC-coupled to the distant device through a 0.1-µF capacitor. This pin provides LVDS signals. Additional components can be required for the optical transceiver. |
15 | SOP | O | Analog | |
16 | SIP | I | Analog | Differential SGMII or Fiber Data Input: This signal carries data from the MAC, fiber transceiver, or link partner, to the PHY in SGMII and fiber modes. This pin is AC-coupled to the distant device through a 0.1-µF capacitor. This pin accepts LVDS signals. Additional components can be required for the optical transceiver. |
17 | SIN | I | Analog |