SNLA467 July 2024 TDP2004
In the following examples, assume that SMBus secondary address 0x18 is used for Device 0 (Channels 0-3) and SMBus secondary address 0x1A is used for Device 1 (Channels 0-3). Example code using TotalPhase Aardvark I2C controller