SNLA468 July 2024 TDP2004
PIN NAME | PIN NUMBERS | PIN DESCRIPTION | RECOMMENDATION | ADDITIONAL PIN CONSIDERATIONS |
---|---|---|---|---|
Main Link Input Pins | ||||
RX[0:3] P/N | 30, 29, 33, 32, 37, 36, 40, 39 | DisplayPort main link differential input | AC-coupled connection from GPU to the TDP2004 | In the case of the DP connector connected to the TDP2004 input, the AC-coupling cap can already be populated on the GPU side. If so, then the TDP2004 input can be DC-coupled. If the TDP2004 input is still AC-coupled, please make sure the total capacitance does not violate the DP specification. |
Main Link Output Pins | ||||
TX[0:3] P/N | 19, 20, 16, 17, 12, 13, 9, 10 | DisplayPort main link differential output | 75nF to 200nF AC-coupled connection from the TDP2004 to the sink or the connector | |
Control Pins | ||||
MODE | 25 | Selects between configuration modes: L0: Pin-strap mode L1: SMbus/ I2C primary mode L2: SMBus/ I2C secondary mode | Tie 1kΩ to ground for pin-strap mode Tie 8.25kΩ to ground for EEPROM control Tie 24.9kΩ to ground for external I2C control | |
DONEn | 7 | Indicates completion of valid EEPROM register load operation. | Only required for SMBus/ I2C primary mode. If not using this mode leave floating | If using SMBus/ I2C Primary mode, external 4.7kΩ pull-up required for operation. |
READ_EN_N | 33 | This pin controls the initiation of the SMBus/ I2C primary mode EEPROM read operation | Only required for SMBus/ I2C primary mode. If not using this mode leave floating | If using SMBus/ I2C Primary mode: After power up, when the pin is low, the device initiates the SMBus / I2C Primary mode EEPROM read function. |
EQ0/ ADDR0 | 23 | In pin-strap mode this pin selects the linear equalization (CTLE) for channels 0-3. This pin is sampled at power-up only. In SMBus/ I2C secondary mode, this pin sets the I2C secondary address. This pin is sampled at power-up only. | Tie 1kΩ to ground for pin-strap mode | See table 6-4 in data sheet for SMBus/ I2C secondary mode |
EQ1/ ADDR1 | 24 | In pin-strap mode this pin selects the linear equalization (CTLE) for channels 0-3. This pin is sampled at power-up only. In SMBus/ I2C secondary mode, this pin sets the I2C secondary address. This pin is sampled at power-up only. | Tie 24.9kΩ to ground for pin-strap mode | See table 6-4 in data sheet for SMBus/ I2C secondary mode |
GAIN/ SDA | 27 | In pin-strap mode this pin selects the flat gain (AC & DC) from the input to the output. This pin is sampled at power-up only. In SMBus/ I2C mode this pin serves as serial data and an external pull-up is required | Leave floating in pin-strap mode | External 4.7kΩ pull up resistor required for SMBus/ I2C mode |
TEST/ SCL | 26 | In pin-strap mode this is a TI internal test In SMBus/ I2C mode this pin serves as serial clock | This needs to be pulled down via a 10kΩ resistor in pin-strap mode | External 4.7kΩ pull up resistor required for SMBus/ I2C mode |
PD | 6 | 2-level logic controlling the operating state of the redriver. Active in all device control modes. The pin has internal 1MΩ weak pull-down resistor. | Leave floating | |
VCC | 14, 15, 34, 35 | Power supply pins. VCC = 3.3V ±10% | The VCC pins on this device must be connected through a low-resistance path to the board VCC plane | Install a decoupling capacitor to GND near each VCC pin |
GND | 1, 8, 11, 18, 21, 28, 31, 38, EP | Ground reference for the device | The exposed pad must be connected to one or more ground planes |