SNLS458B November 2014 – August 2019 DS90UH929-Q1
PRODUCTION DATA.
The DS90UH929-Q1 can detect fault conditions in the FPD-Link III interconnect. If a fault condition occurs, the Link Detect Status is 0 (cable is not detected) on bit 0 of address 0x0C (Table 8). The DS90UH929-Q1 will detect any of the following conditions:
The device will detect any of the above conditions, but does not report specifically which one has occurred.