SNLU131A February 2013 – June 2024
Startup
Make sure all the software has been installed and the hardware is powered on and connected to the PC. Execute Analog LaunchPAD from the start menu. The default start menu location is Programs\National Semiconductor Corp\Analog LaunchPAD vx.x.x\Analog LaunchPAD.
The application comes up in the state shown below. If the application does not, then see Section 4.4. Under the Devices tab click on DS90UH928Q to select the device and open up the device profile and the associated tabs.