The EVM can be used in LDO operation by providing power by using power supply turrets or USB connector. The following jumper connections need to be connected to configure the board for LDO operation.
- For Turret, connect jumper to position 2-3 on J2 connector (pictured) as shown
in Figure 2-3 and
supply power through ‘5V-12V’ and ‘GND’ turrets.
- For USB power, connect jumper to position 1-2 on J2 connector as shown in Figure 2-3 and
supply power through J1 USB connector.
- On the VDD3V3, VDDIO, and MSP-IO connections, make sure that the jumpers are
populated on position 1-2 for all three connectors shown in Figure 2-4.