The MCT8316ZTEVM requires a power supply source, which has a recommended operating range from a 4.5 V to 35 V. To setup and power the EVM, use the following the sequence:
- Connect motor phases to A, B, and C on connector
J13.
- Connect Hall sensors to J11 and select Hall power
supply as 3.3 V from buck or an external Hall supply on J12.
Ensure the MODE resistors are set correctly to use the
appropriate Hall sensor configuration as described in Section 4.6.
- If using digital Hall inputs, populate J8–J10
with shunt jumpers to enable pullups. Connect the
single-ended inputs to only the HPx pins on
connector J11. This is the default of the
MCT8316ZTEVM.
- If using analog Hall inputs, remove J8-J10 and
connect differential Hall inputs to HPx and HNx on
connector J11.
- Ensure resistors are populated in H/W variant
resistors for desired hardware settings.
- Do not turn on the power supply yet. Connect the
motor supply to VBAT or VM and PGND on connector J7.
- To enable reverse polarity protection and Pi
filter, connect to VBAT. Note that when connecting
to VBAT, VM will be VM – 0.7 V less, due to a
diode drop in the reverse-polarity protection
circuit.
- To disable reverse-polarity protection and the Pi
filter, connect to VM.
- Select J3 to 5V_USB and J5 to 3V3COM to power
MSP430 from USB power supply.
- Connect the micro-USB cable into the
computer.
- Turn the potentiometer fully clockwise to set the motor to zero speed upon powerup.
- Turn on the motor power supply.
- Use the potentiometer to control the speed of the
motor and the switches to disable the motor driver, change
the direction, or apply a brake to the motor. Optionally,
use the GUI (as shown in Section 6)
to monitor real-time speed of the motor, put the MCT8316ZT
into a low-power sleep mode, and read status of the
LEDs.