Download the latest version of
Code Composer Studio. This sets up a folder at the directory
C:\ti.
Accept all agreements,
default install locations, and select Next to proceed through
menus.
In the Select
Components window, make sure to check MSP430 Low-Power
MCUs to install the required packages for the MSP430 LaunchPad
Evaluation Kits.
After installing, run CCS and
select a folder or the default to use as the workspace to store any new
projects. The location and naming convention can be changed based on the user's
preference. Click the OK button to accept.
In CCS, click on the Project tab
and select Import CCS Projects. Click on Browse. Select the folder
created in step 1 by extracting the MCT8315Z firmware.
Import the project into the
workspace as shown in Figure 4-3.
Figure 3-3 MSP430FR2355 Interface
Firmware Code in Code Composer Studio