SNOA943 January 2016 FDC2112 , FDC2112-Q1 , FDC2114 , FDC2114-Q1 , FDC2212 , FDC2212-Q1 , FDC2214 , FDC2214-Q1
A second important technique to reduce power consumption in the FDC is gating of the external reference clock. Simply put, the reference clock is also put into a sleep state whenever the FDC is placed into a sleep state. This not only reduces the power consumed by the external clock, but also significantly reduces the leakage current from the FDC.