SNOSD82D June 2018 – September 2022 TMP117
PRODUCTION DATA
The built-in therm and alert functions of the TMP117 can alert the user if the temperature has crossed a certain temperature limit or if the device is within a certain temperature range. At the end of every conversion, including averaging, the TMP117 compares the converted temperature result to the values stored in the low limit register and high limit register. The device then either sets or clears the corresponding status flags in the configuration register, as described in this section.