SNOSD98A May 2020 – December 2020 LM7481-Q1
PRODUCTION DATA
The enable pin allows for the gate driver to be either enabled or disabled by an external signal. If the EN/UVLO pin voltage is greater than the rising threshold, the gate driver and charge pump operates as described in Charge Pump section. If EN/UVLO pin voltage is less than the input low threshold, V(ENF), the charge pump and both the gate drivers (DGATE and HGATE) are disabled placing the LM74810-Q1 in shutdown mode.
If V(ENF) < V(EN/UVLO) < V(UVLOF) then only HGATE is disabled disconnecting the load from the supply, DGATE remains ON.
The EN/UVLO pin can withstand a maximum voltage of 65 V. For always ON operation connect EN/UVLO pin to VS.